FB#.ROLLOVERWEN
Description
This parameter enables the feedback rollover warning W4x32.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-13-01-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 – disabled,1 - enabled |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
FB1.ROLLOVERWEN |
3500h |
22h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB2.ROLLOVERWEN |
3501h |
22h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
30900 |
1 |
30900 (0x78b4) |
FB1.ROLLOVERWEN |
Unsigned8 |
Read/Write |
Yes |
|
30901 |
1 |
30901 (0x78b5) |
FB2.ROLLOVERWEN |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
FB1.ROLLOVERWEN |
30900 |
Unsigned8 |
Read/Write |
- |
|
FB2.ROLLOVERWEN |
30901 |
Unsigned8 |
Read/Write |
- |